skip to content

logo

Sealing of the Belgian symbol: the ATOMIUM

ERIKS_performance_the_ATOMIUM

Problem

The Atomium is the Belgian symbol from the world expo 1958 and  is for the Belgians what the Eifeltower is for the French. The building is 100 m high and exists of 9 balls full of windows. The rubber seals of the windows needed a face lift and for the measurement of the right profile ERIKS engineers hang 80m high above the ground and this at +2°C!

Solution

We succeeded in drawing the right rubber profile and today the Atomium is looking great again at night. Thanks to ERIKS this symbol is alive again bringing emotions to his visitors.

Performance EN