Material Data Table

The Material Data Table is a react component fetching data from an application endpoint exposing data about different materials used to built different ERIKS products, these materials have a set of characteristics relevant to clients including hardness, temperature resistance and approvals.

Details about these materials are imported from PIM periodically and a data structure is built in AEM in order to render this data in the table, if some details are missing or outdated the data should be reviewed instead of the data table component.

Configuration

  • Component dialog can be used to setup the component source, the materials source folder is selected by default and the author can browser the folder and select the structure group to be used to fill in the data in the table.
Material data table dialog image

General contact ERIKS Global Head Office

Location

ERIKS NV
De Entree 239-245
1101 HG Amsterdam
The Netherlands

Find your local ERIKS contact

Chamber of Commerce

37 01 32 89

VAT Number
NL003.076.490.B02