skip to content

logo

Power transmission - CSR

Corporate Social Responsibility means taking into account the effects that the company has on the environment and on the people inside and outside the organisation. As a leading industrial service provider, our operations are not only focused on achieving financial goals but are also emphatically focused on the social and environmental aspects of our activities.

In the position of supplier of a high-quality range of technical components, ERIKS is obliged to give meaning to a strong environmental policy. Environmental aspects are taken into account, both in our own operations as well as in product development and advising clients. New social insights and stricter environmental laws and regulations are being monitored closely. This has led to increased attention for energy savings and the limitation of environmental risks at ERIKS as well as its clients.

Click on one of the CSR case studies of power transmission in the overview below, or go to an overview of all CSR case studies of ERIKS.

  • Fenner saves Christmas

    Fenner saves Christmas

    During the busy Christmas rush an inverter failed on the trifle line of a food manufacturing site in Lincoln. An application engineer of ERIKS UK came up with a solution which reduced the downtime costs to a minimum and which assured the English of their dessert.

  • Saving energy in green houses

    Saving energy in green houses

    Horticulturists save energy The HortiAir is an air treatment system for the climatisation in green houses, developed through thorough cooperation of several specialists. ERIKS Motion Control Schoonhoven supplied the expertise for the controlling of the actuators in the system. With less energy costs an substantial extra production was achieved.

This is a printed version of ERIKS nv.
© ERIKS nv, 2017.