skip to content

logo

Plastic semi-finished products - CSR

Corporate Social Responsibility means taking into account the effects that the company has on the environment and on the people inside and outside the organisation. As a leading industrial service provider, our operations are not only focused on achieving financial goals but are also emphatically focused on the social and environmental aspects of our activities.

In the position of supplier of a high-quality range of technical components, ERIKS is obliged to give meaning to a strong environmental policy. Environmental aspects are taken into account, both in our own operations as well as in product development and advising clients. New social insights and stricter environmental laws and regulations are being monitored closely. This has led to increased attention for energy savings and the limitation of environmental risks at ERIKS as well as its clients.

Click on one of the CSR case studies of plastic semi-finished products in the overview below, or go to an overview of all CSR case studies of ERIKS.

  • Anti-slip protection of stairs

    Anti-slip protection of stairs

    In big football stadions and big buildings the protection of stairs is important. PVC profiles are mostly used to protect the concrete. Due to UV resistance problems the lifetime of this material is reduced to one Year.

  • Tata Steel saves maintenance costs

    Tata Steel saves maintenance costs

    Disturbances of the hot rolling strip mill caused stagnation of the factory. The improvements ERIKS suggested lead to a considerable prolongation of the tool life of the bearings and a higher reliability of the installation.

  • Wheelchairs

    Wheelchairs

    Wooden panels in wheelchairs caused bacterial growth. ERIKS engineers developed a high-quality alternative.

This is a printed version of ERIKS nv.
© ERIKS nv, 2017.