skip to content

logo

Clambing of transported glass

ERIKS_performance_clambing_transported_glass

Problem

Big glass panels are transported over the road and there is a big risk for breaking the glass. So the big glass panels have to be secured and the vibration damped. The rubber used should have low compression set, temperature resistant, soft, antidamping and be selfadhesive one side.


Solution

Our engineers developped a quality which solves all these eventual problems. The ERIKS quality HY/EPDM fest had the best results and some €20.000,- a year is ordered.

Performance EN

"*" denotes required fields. Unfortunately, we will not be able to process your response if these fields are not filled out.

This is a printed version of ERIKS nv.
© ERIKS nv, 2013.